Component Carrier (Basic LTE-A PRACH)

In the figure below, a Basic LTE-A PRACH carrier is selected for configuration. Parameter setup tables for this carrier are described in the following topics:

General (Basic LTE-A PRACH)

Baseband (Basic LTE-A PRACH)

Carrier Configuration Summary Table

This table enables you to view the key parameters for each carrier in the waveform. You can add or delete carriers using the buttons above the table (see descriptions below). To activate the setup tables for a carrier, double-click that carrier row. You can use a maximum of 16 carriers.

Click the Predefined Carrier button to open a window with a list of pre-defined carrier. To replace the current configuration in the setup table with one of these pre-defined configurations, select the desired configuration and click OK or double-click the desired carrier configuration.

Click the Add Carrier button to open a drop-down list from which you can select a carrier to add to the setup table. The carrier is inserted above the currently selected carrier in the table. The maximum number of component carriers is five.

Click the Delete Selected Carrier(s) button to delete the currently selected carrier(s) in the setup table. To select multiple carriers, hold down the CTRL key while you click the desired carriers. You can also use the mouse and the SHIFT key to select a group of consecutive carriers. 

Click the Copy Carrier button to quickly add a copy of the selected carrier to the carrier configuration summary table.

Graph View

The graph view displays several different representations of the generated waveform. For more information, see Graph View.